Germany
 
de
en
 
Germany
 
de
en
 

LAPP launches its first bio-cable in series production


Data cable made of bio-based sheath material

The ETHERLINE® bioP Cat.5e from LAPP is the first LAPP cable with a bio-based sheath material to be produced in series.

Stuttgart, 11 April 2024 – For LAPP as a family business, climate protection has always been part of our DNA. As a result, the company is constantly working on continuing to improve the carbon footprint of its own products and processes – especially for copper and plastics. While copper already uses large quantities of secondary raw materials, LAPP is now working intensively on the sustainable optimisation of sheath materials and is further promoting the use of bio-based plastics.

Last year, LAPP already presented the first prototypes of cables with bio-based sheathing. "Thanks to the complex manufacturing process, sustainable materials are currently considerably more expensive. It was therefore important to us to find out whether our customers are also willing to invest in sustainable products", says Christian Illenseer, Product Manager Automation at LAPP. There was a great deal of interest. LAPP is now going into series production with the ETHERLINE® FD bioP Cat.5e. The data cable consists of a partially bio-based sheath material. The sustainable variant with a bio-based outer sheath consists of 43 per cent renewable raw materials (in accordance with ASTM D6866). The product properties are the same as for the standard variant made of purely fossil raw materials. This reduces the carbon footprint by 24 percent compared to the fossil-based TPU sheath.

Bio-TPU outer sheath for demanding applications


Both the fossil and bio-based variants are suitable for patch cable assembly up to a cable length of 60 m in particularly demanding applications: for example, for constantly moving use in cable chains, in moving machine parts or also for EtherCAT and EtherNET/IP applications. Thanks to its Cat.5e performance up to 1000 Mbit/s, the ETHERLINE® FD bioP Cat.5e enables lightning-fast information exchange and is used to transmit analogue and digital signals in the frequency range up to 100 MHz. In addition, the copper stranded shielding with a high degree of coverage guarantees optimum protection against electromagnetic interference. Halogen-free and flame-retardant materials reduce the possible hazards in the event of a fire. In addition, the Bio-TPU outer sheath is insensitive to mineral oil-based lubricants and is chemically resistant in many cases. The highly flexible Cat.5e Ethernet cable has been successfully tested in LAPP’s own test centre for over 1 million bending cycles in the cable chain. UL/CSA certification in accordance with the technical data also allows the product to be used in North America.

Next prototype in the pipeline


The next more sustainable variant is the ÖLFLEX® CLASSIC FD 810 in the pipeline. An initial prototype was recently unveiled.  The challenge: it is not yet technically possible to produce polyvinylchloride - PVC for short - entirely on the basis of bio-based raw materials. One starting point is therefore a partially bio-based sheath made of PVC compound, the bio-based content of which is 42 per cent according to ASTM6866. "The ÖLFLEX® CLASSIC FD 810 is a very versatile cable that is also designed for cable chains. It can additionally be used to test the cable chain properties of the material. It therefore offers us a wide range of tests for carrying out material tests for certifications," says Alexander Terpe, Head of Product Development Cables at LAPP.

Incidentally, in production, LAPP is already working on ideas for recycling secondary materials from plastic waste. They are intended to be used, for example, as a filler in the cables.