How LAPP steers the future
Companion for a digital world
Stuttgart, 16 February 2022 - Digitalisation, customisation, miniaturisation and automation are the major trends in the industry. LAPP is also addressing these future issues. "Innovative is one of LAPP's values. But we have recognised that we need to work and think differently today if we are to drive innovations creatively and efficiently. This includes having to think outside the box and striving to offer solutions and services that go beyond the further developing cables and connectors in the future", asserts Georg Stawowy, Member of the Board for Innovation and Technology at Lapp Holding AG.
LAPP has now presented a new solution for predictive maintenance in the Smart Factory. ETHERLINE® GUARD is a stationary monitoring device that uses patented predictive maintenance algorithms to assess the momentary performance of data cables subject to particular stress. ETHERLINE® GUARD thus contributes to realising a "digital twin" within production facilities. "For LAPP, this is a paradigm shift, as it involves embedded software and programming an algorithm. This is something completely different to developing a cable", Georg Stawowy stresses and adds: "Creating a digital picture of the physical world is a mega trend that we have also embraced in the field of connection solutions".
LAPP presented a prototype of ETHERLINE® GUARD in its futureLab at the Hannover Fair 2019. This was an initial laboratory model. The basis for this was a new, agile innovation process, called Innovation-For-Future, which for the first time offers a systematic framework for radical and disruptive innovations. Unlike the classic Stage-Gate process, the Innovation For Future process will be carried out if the intended product is not yet clearly defined at the outset. For this reason, an initial functional prototype has to be developed in sprints for series production and with regular customer feedback. LAPP has defined three prerequisites here: An initial prototype must be in place, this prototype must have been assessed for added value by at least one customer, and an initial idea for the business model must have been developed. The Innovation for Future process gives us the freedom to drive forward innovations outside our core business.
The early introduction of ETHERLINE® GUARD to potential customers was extremely helpful for LAPP in the development process. As early as 2020, ETHERLINE® GUARD was used by three pilot customers from the medical technology, automotive and intralogistics sectors, as well as in the LAPP service and logistics centre in Ludwigsburg. Thanks to direct customer feedback, it was possible to prevent the innovation from being developed without clearly focusing on the industry. So, simple operation yet complex functionality were particularly important to customers. The fully marketable product was finally launched three months ago. ETHERLINE® GUARD is in particular demand from customers for whom a malfunction or repair of a cable would be particularly critical and costly. LAPP envisions applications in the process industry, the automotive sector, medical technology and critical supply infrastructure.
ETHERLINE® GUARD and the associated evaluation of a cable’s performance data for predictive maintenance is just the first step for LAPP. In the future, LAPP is looking to use this digital lifecycle of a cable in much more diverse ways and also to directly offer customers such performance profiles for developing new machines and systems. "The software and algorithm allow us to represent the behaviour of a cable in the digital twin. This means that a machine tool's operation under load can firstly be simulated with a purely virtual method. We can digitally represent the entire production process. This enables wear, design improvements and maintenance intervals to be taken into account during the development process. That is the future," says Georg Stawowy.