Germany
 
de
en
 
Germany
 
de
en
 

LAPP will be exhibiting at LogiMAT 2024


Optimally networked and smartly automated


Stuttgart, 07 February 2024 – Global megatrends such as digitalisation and automation are changing our world. This can be seen in all industries and, in particular, in intralogistics, which is becoming increasingly networked and requires new approaches. LAPP will be bringing answers to the associated challenges at LogiMAT 2024 in Stuttgart. The connection solutions from the global market leader can be seen in Hall 3, Stand F60.

Europe’s largest international trade fair for intralogistics solutions and process management is setting new standards. At the trade fair site in Stuttgart, it offers a complete market overview of everything that moves the industry. Combined under the trade fair slogan "Shaping Change Together", international exhibitors will be presenting innovative technologies, products, systems and solutions on the topics of digitalisation, networking, artificial intelligence and big data in intralogistics. The portfolio of LAPP, the leading supplier of connection solutions and branded products in the field of cable and connection technology, should not be missing here either.

High-quality components for optimum data flow


Intralogistics has long become a central topic at LAPP. From power and control cables to connectors and cable glands or cable protection and routing systems, the Stuttgart-based company has everything you need for an optimum connection solution in this area.

As complexity increases, so do the challenges for products and solutions, such as high-performance data networks. They transport a valuable commodity that must be transmitted reliably and at the optimum time between all components of a data network. To meet this challenge, LAPP offers solutions from a single source and is focusing on comprehensive networking of data and processes at LogiMAT 2024 in order to increase transparency and efficiency in intralogistics. The industrial, robust and high-quality components for networking factories, machines or plants are paving the way for customers to achieve Industry 4.0 and guarantee safe and reliable transmission of data and power, even under significant chemical, mechanical or thermal loads.

In order to ensure that the intralogistics of the future does not just remain an idea, but works seamlessly across different levels, it is important to have uniform communication between the various participants within one or more networks. At LogiMAT 2024, experts from LAPP will be presenting clever solutions based on the leading protocol standard PROFINET as well as all other standards.

ÖLFLEX® CONNECT CHAIN: One for all


Automated high-rack warehouses are increasingly becoming the standard for intralogistics. Here too, LAPP thinks along with you and brings its complex and proven drag chain systems to the logistics trade fair. With ÖLFLEX® CONNECT CHAIN, the company has a fully pre-assembled drag chain system in its repertoire that can be tailored precisely to a wide variety of applications. At the LAPP trade fair stand, customers will have the opportunity to receive comprehensive advice on a tailored solution, from motor connection cables to pre-assembled cable chains or assemblies.