Germany
 
de
en
 
Germany
 
de
en
 

Optimise intralogistics with LAPP


LAPP exhibits at the LogiMAT 2025 in Stuttgart

UNITRONIC® ACCESS - IO-Link technology significantly reduces the amount of wiring required.

Stuttgart, 06 February 2025 - The demands on intralogistics are constantly increasing: automation, digitalisation and artificial intelligence are shaping the industry. From 11 to 13 March 2025, the international trade fair LogiMAT in Stuttgart will provide an overview of the latest developments and trends. LAPP, the leading supplier of cable and connection technologies, will be there in Hall 3, Stand A19, providing innovative solutions for greater efficiency, flexibility and safety in intralogistics.

Intralogistics has long been one of LAPP's specialities. Because all requirements for increasing flexibility, innovation or speed, automation and robotics have one thing in common: they require a secure and reliable data and energy supply that can be adapted modularly and intelligently to all requirements.

LAPP as a key player for the intralogistics of the future


Efficiency, transparency and networking are the success factors of modern intralogistics - and LAPP supplies the essential infrastructure for this. This includes solutions for the smooth running of warehouse operations, for example through connectable cable sets or a comprehensive product portfolio for all common protocol standards, as well as servo assemblies and drag chain solutions for the optimal flow of goods from the raw materials warehouse through production to the finished product. With high-quality cabling solutions, the company ensures the reliable connection of automated storage and transport systems, enabling time and cost savings. Robust, flexible and durable cables from LAPP can cope with even the most demanding industrial conditions and guarantee continuous data communication - the lifeblood of smart logistics processes.

LAPP also offers predictive maintenance solutions, a pioneering technology that uses sensors and data analysis to identify maintenance requirements at an early stage and minimise downtimes. This makes LAPP a reliable partner for all those who want to take their intralogistics to the next level. For example, LAPP's eKanban system, which supports customers with digital and intelligent cable inventory management in real time, will also be on the stand. This smart predictive maintenance solution informs users in real time when components should be replaced - for greater operational reliability and fewer unplanned downtimes.

However, the Stuttgart-based company offers many more products and solutions for intralogistics, such as the new remote I/O devices from LAPP, with which the connectivity provider is expanding its portfolio with a smart solution for the seamless connection of sensors and actuators to automation systems. At the LAPP trade fair stand, users can find out how IO-Link technology significantly reduces the amount of wiring required, while plug-and-play makes commissioning much easier. The devices offer maximum flexibility, especially for intralogistics, as they support common protocols such as PROFINET, Ethternet/IP and Modbus TCP. The UNITRONIC® ACCESS series includes powerful IO-Link masters and hubs that can be conveniently configured via web interfaces. Reliability and durability are the focus here - quality "Made in Germany" makes the solution a real added value for automation processes.

A package of services and products - LAPP Harnessing Solutions


Another highlight of the trade fair appearance will be the LAPP Harnessing Solutions - an all-round carefree package that is perfectly tailored to the requirements of intralogistics and includes the CABLES, SERVO, CHAIN and Boxbuild services. From development and documentation through to series production, LAPP offers customised solutions that guarantee maximum efficiency and reliability.