United Kingdom
 
 
£
United Kingdom
 
 
£

SKINTOP® cable glands

Insert the cable, tighten - done!

Secure and Effective


SKINTOP® was launched on the market in 1978 as a revolutionary cable gland: insert the cable, tighten, done! Today, the extensive SKINTOP® range of cable glands fulfils almost all application requirements and offers unrivalled advantages. Discover SKINTOP®!

Download flyer

voucher code*: SKINTOP10

Experience the proven SKINTOP® quality for yourself – Get our original now with an attractive price advantage
Shop now

We're happy to help

Do you have any questions about SKINTOP® cable glands? Ask our experts!
Ask us

The benefits of SKINTOP® cable glands


  • Optimum strain relief thanks to the extreme wide clamping range that secures, centres and prevents the cable from being pulled out, even with strong movement in the application
  • Permanent protection against vibration: intensively tested for the toughest application
  • Maximum sealing against environmental influences such as dust, dirt and water
  • Secure connection: cables are secured, centred and hermetically sealed
  • Installing a SKINTOP® cable gland is extremely easy
  • High resistance to oil, UV and ozone

Discover the SKINTOP® cable glands


SKINTOP® has a very wide range of glands. The wide range meets almost all application requirements. View the entire product range here.

A SKINTOP® gland for every application

The temperature essentially determines the current properties of a material. Make sure that the specified temperature ranges are adhered to when using our products. Don't get caught off guard

For extreme sub-zero temperatures of up to -70°C, you can rely on cold-resistant LAPP cable glands such as the SKINTOP® COLD. For extreme plus temperatures of up to +200°C, we recommend the SKINDICHT® SHV-M FKM.

If a cable or wire is used in moving machine parts, the minimum bending radius of the product must be observed. The SKINTOP® BS-M helps, for example, with its shape preventing the cable or wire from kinking on the cable gland.
Depending on the application area, a cable gland comes into contact with substances that can attack the gland material.

Cable glands with flame-retardant properties are absolutely relevant to safety in areas with high potential hazard in the event of a fire. Cable glands with halogen-free and highly flame-retardant components are therefore suitable for areas at risk of fire. They reduce the risk of flame propagation, high smoke density and toxic flue gases in the event of a fire.

In rail vehicles in particular, the fire behaviour of all installed components is strictly tested. EN 45545-2 contains the technical requirements for these components.

The UL 94, a testing method for the flammability of plastics, divides the plastics into flammability classes and is often requested when plastic cable glands are used.

SKINTOP® ST-HF-M

Smooth surfaces and contours without corners or edges prevent residues such as liquids and micro-organisms from accumulating on a cable gland and there is a risk of contamination for food in the processing facility. As all food processing plants are regularly cleaned with hot water or water steam or by foaming and aggressive disinfectants are used, standard suitability for the food industry is only achieved using stainless steel cable glands.

  • Please ensure certification in accordance with the EHEDG (European Hygienic Engineering and Design Group) standard if the cable gland is to be used in hygiene-critical areas.
  • The National Sanitation Foundation (NSF) specifies the NSF/ANSI 169 - 2016 standard for materials intended for use in the food industry in the USA.
  • ECOLAB Inc. is a manufacturer of cleaning agents and disinfectants for the gastronomy, food industry and agriculture. The ECOLAB® certification is recognised worldwide. ECOLAB® certified cable glands are resistant to ECOLAB® disinfectant and cleaning agents.

SKINTOP® HYGIENIC

In chemical factories or filling stations, explosive gases can form, for example during the generation and filling of fuels. However, precautions must also be taken in the production of sugar and flour to prevent dust explosions. In order to be able to rule out any ignition source, all construction materials used in this particular environment must have their properties comply with the standards that have been set up to prevent accidents.

ATEX stands for “ATmosphères Explosibles”. The LAPP cable entries with the addition "ATEX" meet the explosion protection requirements in accordance with DIN EN IEC 60079-0 and DIN EN IEC 60079-7 and are therefore suitable for use in explosive atmospheres (ignition protection type "Enhanced safety" ("e")).

SKINTOP® K-M ATEX plus

Single Entries

For a secure fit in no time at all!

Get our original now with an attractive price advantage. 

Use the code*: SKINTOP10

Multi-entry systems

For many cables, but zero chaos.

Get our original now with an attractive price advantage

Use the code*: SKINTOP10


*The voucher of 10% can be redeemed between 17 February and 15 April 2025 on an order in the online shop at www.lapp.com/en/de and is only valid for SKINTOP® cable glands exkl. accessoires. The voucher can be redeemed once per customer number. The voucher is not valid for purchases already made or exchanged items and cannot be combined with other vouchers or promotions. The voucher cannot be redeemed on "My offers" in the online shop. U.I. Lapp GmbH reserves the right to terminate the validity of the voucher prematurely or to withdraw the voucher in the event of misuse. Our general terms and conditions for the U.I. Lapp GmbH online shop apply to purchases.