Germany
 
de
en
 
Germany
 
de
en
 

LAPP expands its portfolio of EPIC® POWER M12 connectors


Here come the EPIC® Minis

Small and powerful: the new EPIC® POWER M 12K 4A circular connector

Stuttgart, 24 April 2023 - The smallest power plug from LAPP has a new addition. At its spring 2023 launch, the global market leader for integrated solutions in the field of cable and connection technology will be presenting its new circular connector EPIC® POWER M12 K. The LAPP portfolio of mini-power connectors has thereby been enlarged.

The trend towards miniaturisation doesn't stop at connectors. In many areas of industry, applications are becoming smaller and smaller, while power density is increasing. Connectors are also obliged to follow this trend. In automation technology in particular, both faultless data transmission and reliable power supply to individual components are sensitive issues. PROFINET places its full trust in the standardised M12 L connector. EPIC® POWER M12 plug connectors from LAPP are the logical answer to this market requirement.  

The new EPIC® POWER M12 K for conductor cross-sections of 0.75 to 2.5 mm2 is primarily suitable for connecting three-phase motors of up to 7.5 kW or for supplying power to devices and machines in a wide range of applications. It also guarantees optimum electromagnetic compatibility and can withstand high environmental and mechanical loads. And besides this it has ample power! The mini power connector of the M12 K series is suitable for power transmission of up to 630V/12A. The mechanical K coding of the connector face prevents it being plugged incorrectly into the mating connector. And in connected state, it can attain protection class IP 65, IP 67 and IP 69.

EPIC® POWER M12 L connector up to 16 A

The EPIC® POWER M12 K is the logical addition to the new EPIC® POWER M12 L connector, which has been developed for power transmission of up to 60V/16A. Use in I/O modules for PROFINET is an important field of application for the EPIC® POWER M12 L plug connector. To date, 7/8" plug connectors have been the standard power interface for the sensor/actuator control cabinet. The change from the old standard to the M12L enables boxes to be reduced in size by over 50%. The PNO has defined the L-coded M12 as the interface for the power supply for all PROFINET applications. This is the set standard for PROFINET devices such as intelligent motors or I/O modules. M12 L coding offers the ideal conditions for this.

During development, the technical properties of the smallest connectors were simulated based on virtual models. The two M12 K series for energy transmission up to 630V/12A and M12L up to 60V/16A were put through their paces virtually in this way before the first 3D-printed model was produced. This means that the limit of power transmission with increasingly smaller connectors was first evaluated virtually and then transferred to initial prototypes and series production. "The previous M12 plug connectors were already developed very close to the limits of feasibility. We have now checked all factors once again to achieve the best results. This would barely have been possible without the virtual design,” stressed Steffen Schneider, Product Manager at U.I. Lapp GmbH. The unbeatable results of the EPIC® Minis are significantly smaller sizes and improved power transmission.